Technical FAQs

Ask a Question

What is the part number for the fan on the Omegapak 8804 CT (125-250hp), EVT & VT (150-300hp) ?

The part number is 26016-31100 for the heatsink fan which has quantity of 3 per drive. The part number for the door mounted fans is 26016-30620 which has a quantity of 2 per drive.


CTA-ID : 4137
Was this helpful?
What can we do to improve the information ?