Technical FAQs

Ask a Question

Can you get a remote operator with a reset button for the Omegapak 8804 unit?

The digital operator interface (DOI) is available. Would have to get the following parts:
DOI interface board 52011-827-50
DOI Cables (C frame) 52011-837-51
DOI display 52011-850-50
Serial Com board 52011-405-50

CTA-ID : 4131
Was this helpful?
What can we do to improve the information ?