Technical FAQs

Ask a Question

Why can`t we get the Omegapak 8804 serial communication board to communicate with the DOI?

Is the serial communication board rev M. We would need the version of the Eprom memory. Does the Eprom have a funny part number such as 52011-533-50. That version was not made to communicate with a DOI. It was for PLC communications only.


CTA-ID : 4130
Was this helpful?
What can we do to improve the information ?