Technical FAQs

Ask a Question

What is the part number of a square legend plate to use with the 9003KBA1A operator?

Can`t use this type of legend with this operator. Need operator with 45 x 45 or 60 x 60 mm square bezel.


CTA-ID : 4956
Was this helpful?
What can we do to improve the information ?