Technical FAQs

Ask a Question

Are the class CC and J fuses fuses fast or slow acting that are recommended for use on the Altivar ATV18?

Class J fuses are fast-acting and Class CC are time delay but they are chosen according to the amount of current and voltage it lets through before it clears.


CTA-ID : 4400
Was this helpful?
What can we do to improve the information ?