Technical FAQs

Ask a Question

Can we use a MG breaker in front of the Altivar ATV18 drive instead of fuses.

You have to use fuses on the front end of the drive, circuit breakers do not open fast enough to clear a fault such as how unit was tested with the fuses.


CTA-ID : 4396
Was this helpful?
What can we do to improve the information ?