Technical FAQs

Ask a Question

Does the Altivar ATV18 unit have a keypad capable of allowing remote control?

Issue:  Does the Altivar ATV18 unit have a keypad capable of allowing remote control?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  N/A
 
Resolution:  The keypad part number INV162 which is offered by third part Prizm at 724-941-3200 does allow for remote keypad control.


 
Was this helpful?
What can we do to improve the information ?