Technical FAQs

Ask a Question

Why does the black connector for DOI with bundled wires not fit into the board because the pins appear not to be long enough on the 52011-038-253 component of the Omegapak 8804.

A few boards had got out that had the pins too short. Need to send the main control board in for a replacement.


CTA-ID : 4127
Was this helpful?
What can we do to improve the information ?