Technical FAQs

Ask a Question

Can control board part number 52011-038-50 for the Omegapak 8804 be repaired?

Boards possibly can be repaired depending upon the extent of the damage it has sustained, but have to go through depot which can determine whether repairable or if need replacement.

CTA-ID : 4126
Was this helpful?
What can we do to improve the information ?