Technical FAQs

Ask a Question

What needs to be set to put the overload to no more than 99% on the EVT Omegapak 8804?

Adjust the P7 pot on the drives MCB in order to scale the overload properly from 75-120%. Do not know what voltage value to take from terminals 30 & 31 on the MCB.


CTA-ID : 4124
Was this helpful?
What can we do to improve the information ?