Technical FAQs

Ask a Question

Does the Max Speed potentiometer on the Omegapak 8804 control both auto and manual speed reference signals maximum frequency?

Yes it does. If it is changed and want to run in DOI mode will want to recalibrate the DOI.

CTA-ID : 4122
Was this helpful?
What can we do to improve the information ?