Technical FAQs

Ask a Question

What is part number - 52011-002-01 that is on an Omegapak 8804 unit for?

52011-002-01 is the number on the silk screen of the gate driver board. The correct part number for the board would be 52011-003-50.

CTA-ID : 4118
Was this helpful?
What can we do to improve the information ?