Technical FAQs

Ask a Question

Customer asking if the ZCKE05 has an ``O``Ring? Can I get the deminsions of the O-ring?

There is no O-ring on the operating head, but there is one on the body. O-ring is as measured as - outside diameter 1.103 inches X .06 inches thick.

CTA-ID : 4942
Was this helpful?
What can we do to improve the information ?