Technical FAQs

Ask a Question

What type of fusing is to be used on the Altivar ATV18 unit?

Issue:What type of fusing is to be used on the Altivar ATV18 unit?
 
Product Line:ATV18
 
Environment:All
 
Cause:N/A
 
Resolution:Class J or CC Both are fast acting.


 
Was this helpful?
What can we do to improve the information ?