Technical FAQs

Ask a Question

Can the torque limitations go up to 200% on the Altivar ATV18?

Issue:  Can the torque limitations go up to 200% on the Altivar ATV18?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  N/A
 
Resolution:  The torque limitation of 150% for CT is just a function of the current draw. If the drive is upsized for a higher current rating then the torque can be increased as well.


 
Was this helpful?
What can we do to improve the information ?