Technical FAQs

Ask a Question

How do you factory reset the Altivar ATV18 unit?

Issue: How do you factory reset the Altivar ATV18 unit?
 
Product Line: ATV18
 
Environment: All
 
Cause: Factory reset
 
Resolution: First, set parameter L2A to YES so that you can access level 2. Then set parameter FCS to Yes to program the unit for Total factory settings


 
Was this helpful?
What can we do to improve the information ?