Technical FAQs

Ask a Question

Can the Switching frequency be adjusted to 5Khz on the Altivar ATV18?

Issue:  Can the Switching frequency be adjusted to 5Khz on the Altivar ATV18?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  Switching frequency
 
Resolution:  The unit can be adjusted to 5Khz by setting SRf, you must also derate the unit by 5% at that point.


 
Was this helpful?
What can we do to improve the information ?