Technical FAQs

Ask a Question

What is the UL file number for the Altivar ATV18?

Issue: What is the UL file number for the Altivar ATV18?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: The file number is E164874.


 
Was this helpful?
What can we do to improve the information ?