Technical FAQs

Ask a Question

Do I have to use shielded cable for the Altivar ATV18 output leads of the motor?

Using a shielded motor cable is a requirement if the drive needs to be in compliance with EMC directive, typically used in Europe.


CTA-ID : 4373
Was this helpful?
What can we do to improve the information ?