Technical FAQs

Ask a Question

Can the customer use solid state trip device on the output of the Altivar ATV18?

Using solid state devices on the output of the drive is not recommended because the drive has PWM output waveform which does not work well with these devices.

CTA-ID : 4372
Was this helpful?
What can we do to improve the information ?