Technical FAQs

Ask a Question

Does the Omegapak 8804 unit have arcing ground fault protection?

The unit has ground fault detection but if the ground current is so high that it starts arcing it may be too much for the unit to handle.


CTA-ID : 4113
Was this helpful?
What can we do to improve the information ?