Technical FAQs

Ask a Question

What is the trip level for overvoltage and undervoltage on the Omegapak 8804?

Informed that overvoltage trips at 900vdc for 460vac systems. Informed that the tirp level for undervoltage is at 87.5% of rated input voltage, Automatically resets at 95%of rated input votage.


CTA-ID : 4112
Was this helpful?
What can we do to improve the information ?