Technical FAQs

Ask a Question

Is there a better way of replacing the Omegapak 8804 A frame GTO besides sending unit in for possible repair or could the B frame GTO`s be used?

Sending unit in for repair at the depot is the only option since can`t supply the GTO`s anymore. Also informed that can`t substitute the B frame GTO`s for this and they are not available anyway either.


CTA-ID : 4111
Was this helpful?
What can we do to improve the information ?