Technical FAQs

Ask a Question

How can you adjust the mA speed reference output from the unit on the Omegapak 8804?

Without the DC to DC output card the only available speed reference is from terminals 4 & 6 on the mcb which is 0-2.5 volt with maximum speed of 60hz and 0 to 5v with maximum speed of 120hz.


CTA-ID : 4109
Was this helpful?
What can we do to improve the information ?