Technical FAQs

Ask a Question

Are there dipswitches to set the line voltage on an Omegapak 8804?

Issue: Are there dipswitches to set the line voltage on an Omegapak 8804?
 
Product Line: 8804 Omegapak
 
Environment: All
 
Cause: N/A
 
Resolution: There are dip switches to set the line voltage correctly and can obtain this information out of the manual corresponding to the unit you have.


 
Was this helpful?
What can we do to improve the information ?