Technical FAQs

Ask a Question

What is the part number of the module chip for the Omegapak 8804 with DOI ( digital operator interface )?

The DOI module chip part number is 52011-828-50 and it is important to verify the revision letter of chip being replaced because there are compatibility issues if don`t match up properly between keypad, DOI board and serial board.


CTA-ID : 4102
Was this helpful?
What can we do to improve the information ?