Technical FAQs

Ask a Question

Omegapak 8804 with DOI (digtial operator interface) What is the part number of the serial board on the Omegapak 8804 with DOI ( digital operator interface )?

The serial board part number is 52011-405-50 and it is important to verify the revision letter of board being replaced because there are compatibility issues if don`t match up properly between keypad, DOI board and serial board.

CTA-ID : 4101
Was this helpful?
What can we do to improve the information ?