Technical FAQs

Ask a Question

What is the part number of the Omegapak 8804 DOI ( digital operator interface ) interface board?

The DOI interface board part number is 52011-827-50 and it is important to verify the revision letter of board being replaced because there are compatibility issues if don`t match up properly between keypad, DOI board and serial board.

CTA-ID : 4100
Was this helpful?
What can we do to improve the information ?