Technical FAQs

Ask a Question

9007 CLS1, what is the NEMA enlosure rating on this device ?

This device falls under the same enclosure ratings as the std 9007 Type C. NEMA 1, 2, 4, 6, 6P, 12, 13.


CTA-ID : 4912
Was this helpful?
What can we do to improve the information ?