Technical FAQs

Ask a Question

What is the power factor of the Altivar ATV18 unit?

Issue: What is the power factor of the Altivar ATV18 unit?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: The displacement power factor is 96%.


 
Was this helpful?
What can we do to improve the information ?