Technical FAQs

Ask a Question

Where can a fire alarm be wired in on the Altivar ATV56 for a unit without bypass?

Wire it between +24 and LI1 run enable since when this opens the unit will not run in any mode and performs a freewheel stop.


CTA-ID : 4363
Was this helpful?
What can we do to improve the information ?