Technical FAQs

Ask a Question

Is the motor thermal protection parameter ItH on the Altivar ATV18 an actual value or a percentage? Can it be set to 0.5?

It is factory set to the drive rated output current but it can range from 50% to 115% of the drive rated current and the setting is an actual value. No it can not be set to 0.5 but it can be set to 0.5 times the rated current of the unit which is 50%.

CTA-ID : 4360
Was this helpful?
What can we do to improve the information ?