Technical FAQs

Ask a Question

Can customer tell the unit to start when a 120V thermal switch closes which want to connect to the Altivar ATV18 LI1?

No, the logic inputs are rated for 24V(30V max). The 120V switch can not be connected directly to the logic input. Would have to get a 120V relay to connect the switch by interposing.


CTA-ID : 4357
Was this helpful?
What can we do to improve the information ?