Technical FAQs

Ask a Question

Are there additional dry contacts that can be added to the Altivar ATV18 drive?

Issue:  Are there additional dry contacts that can be added to the Altivar ATV18 drive?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  N/A
 
Resolution:  No, there is only SA, SB & SC.


 
Was this helpful?
What can we do to improve the information ?