Technical FAQs

Ask a Question

On a 9007 C54JS7. What does the S7 mean ?

S7 is a suffix for special modification, in this case S7= 8`` delrin extension. The S number is unique for the individual type and class number that it is associated with. Its meaning cannot be applied globally to other type numbers, even within the same class.

CTA-ID : 4904
Was this helpful?
What can we do to improve the information ?