Technical FAQs

Ask a Question

Is the replacement pilot light bulb available for the 2510 KF2C?

This is a sealed unit, complete module part number 9999 PL13 for Red or 9999 PL13G for Green must be replaced. This also applies to 2510 KF4C, 2510 KG2C, 2510 KG4C, 2510 KG6C, 2510 KGJ2C, 2510 KGJ4C, 2510 KO2C, 2510 KO2CT, 2510 KO4C, 2510 KO6C, 2510 KS2C, 2510 KS4C, 2510 KSJ2C, 2510 KSJ4C, 2511 KF22C, 2511 KG22C, 2512 KF22C, and 2512KG22c devices.


CTA-ID : 4621
Was this helpful?
What can we do to improve the information ?