Technical FAQs

Ask a Question

Is there a way to lock the parameters so that no one can change them on the Altivar ATV18?

This unit does not hava a access lock that prevents individules from changing them while setting L2A parameter to no will not allow access to level two parameters.

CTA-ID : 4341
Was this helpful?
What can we do to improve the information ?