Technical FAQs

Ask a Question

What needs to be done if two motors are on one Altivar ATV18 drive? This is not for a slamming application

You will need to add separate overloads. Also size the drive to the total FLA of the two motors.


CTA-ID : 4340
Was this helpful?
What can we do to improve the information ?