Technical FAQs

Ask a Question

Can you use the up and down arrow keys to change the speed of the units?

The Up and Down arrows keys do not change the speed on the unit. The best way to change the speed is by adjusting the low speed if have no analog speed reference connected to unit and unit is running at low speed when give a direction signal.

CTA-ID : 4337
Was this helpful?
What can we do to improve the information ?