Technical FAQs

Ask a Question

Is a ZB3BW13 still available?

The XB3 line was a 30 mm Tele. line. It is no longer available. It used the same contact block, light modules, and lenses as the XB2 line so some parts are still available. Suggest replacing operators, etc. with the 9001 K line.


CTA-ID : 5224
Was this helpful?
What can we do to improve the information ?