Technical FAQs

Ask a Question

How can you run at one speed without using a speed potentiometer?

Set the low speed (LSP) for what you need. then when a run command is given by either putting 24v to forward or to reverse the drive will go to that speed.

CTA-ID : 4336
Was this helpful?
What can we do to improve the information ?