Technical FAQs

Ask a Question

Would the preset speed on the Altivar ATV18 still work if the drive was running in reverse?

Preset speeds work in both the forward and reverse conditions.


CTA-ID : 4332
Was this helpful?
What can we do to improve the information ?