Technical FAQs

Ask a Question

How do I set up 3 preset speeds in the Altivar ATV18?

Issue: How do I set up 3 preset speeds in the Altivar ATV18?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: Told him to first clear all Logic Input settings. Then program LI3 for PS4, then program LI2 for PS2, the sequencing is very important. Then set SP3 and SP4 for the preset speeds.


 
Was this helpful?
What can we do to improve the information ?