Technical FAQs

Ask a Question

Can you power their PLC from the Altivar ATV18 drive +24V source, to supply the 4-20ma input to the drive.

It is not recommended because if you short the +24 or overdraw it, they could damage the power board. Do not want to exceed power supply rating.


CTA-ID : 4326
Was this helpful?
What can we do to improve the information ?