Technical FAQs

Ask a Question

How can you get a signal from the Altivar ATV18 drive when it is running.

Suggested using the LO output set for frequency level attained (FtA). Then select a .1 hz frequency with Fdt. Jumper +24 to LO+ for a power supply. Then using LO to com for a signal that will turn on at start up.

CTA-ID : 4325
Was this helpful?
What can we do to improve the information ?