Technical FAQs

Ask a Question

Can you use a 20 to 4 ma input with the Altivar ATV18?

Issue:  Can you use a 20 to 4 ma input with the Altivar ATV18?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  Analog input
 
Resolution:  Can not use this input signal with this unit.


 
Was this helpful?
What can we do to improve the information ?