Technical FAQs

Ask a Question

Can you use the GV2 as disconnect on the Altivar ATV18?

Issue: Can you use the GV2 as disconnect on the Altivar ATV18?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: As long as the available fault is less than 5,000 amps AIC you can.


 
Was this helpful?
What can we do to improve the information ?