Technical FAQs

Ask a Question

How can you get to level 2 parameters in the Altivar ATV18?

Issue: How can you get to level 2 parameters in the Altivar ATV18?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: You have to use the arrow key to get to the L2A parameter which you then change to yes and then access is permitted.


 
Was this helpful?
What can we do to improve the information ?