Technical FAQs

Ask a Question

Will the Altivar ATV18 drive accept a 4-20ma signal?

Issue: Will the Altivar ATV18 drive accept a 4-20ma signal?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: Yes, 4-20, and 0-10volt will be accepted


 
Was this helpful?
What can we do to improve the information ?