Technical FAQs

Ask a Question

Is the Altivar ATV18 drive single phase in and 3 phase out?

Yes there is a model of the ATV18 that is single phase input and 3 phase output but some of the units are 3-phase in and 3-phase out.


CTA-ID : 4303
Was this helpful?
What can we do to improve the information ?